Technical FAQs

Ask a Question

What is the part number for the N2 Metasys interface card for the Altivar ATV56 drive?

Told him that he will need to order a 66 to be able to host serial communications then will need the IO extension module and will need to contact NR&D for the N2 interface card.

CTA-ID : 6697
Was this helpful?
What can we do to improve the information ?