Technical FAQs

Ask a Question

Why does ATV18 drive say ready but does not run?

Issue: Why does ATV18 drive say ready but does not run?
 
Product Line: ATV18
 
Environment: All
 
Cause: Not running
 
Resolution: Jumper +24 to LI1 so will have a direction signal and with a speed reference present or LSP higher than 0hz the unit will run.


 
Was this helpful?
What can we do to improve the information ?