Technical FAQs

Ask a Question

What are the repair parts for a QO12040M200RB, Series S1 (or S01), Load Center?

Issue:
Design repair parts

Product Line:
QO Load centers

Environment
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4054802203
Interior Trim - 4056309201
Interior Assembly - QO12040M200RBI
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QOM2200VH
Interior Trim Mounting Screw - 4020513001K
RB Door Mounting Screw - 2142717161
Main Circui Breaker and Main Lugs Keps Nut - 2342702001


CTA-ID : 7774
Was this helpful?
What can we do to improve the information ?