Technical FAQs

Ask a Question

How do I add a new style EZM (3-Phase, 4-Wire) branch unit to an existing old style EZM (3-Phase, 4-Wire) metering lineup?

Issue:
Application

Product Line:
EZM

Cause:
Adding new to old style EZM

Resolution:
To add a new style EZM branch unit to the RIGHT side of an existing old style EZM lineup, order an EZM3TRANR transition section and the appropriate EZM branch unit. Note that the transition section is 10.7`` wide.
To add a new style EZM branch unit to the LEFT side of an existing old style EZM lineup, order an EZM3TRANL transition section and the appropriate EZM branch unit. Note that the transition section is 10.7`` wide.unit.


CTA-ID : 7735
Was this helpful?
What can we do to improve the information ?