Technical FAQs

Ask a Question

Do our drives have conformal coating on the electronic boards?

Our electronic boards are rated according to pollution degree specifications brought out in IEC and NEMA standards found in the Environmental Specifications in the manual. They have conformal coating in areas of the board where it is needed to comply with these standards.

CTA-ID : 6455
Was this helpful?
What can we do to improve the information ?