Technical FAQs

Ask a Question

What wire sizes will work with the CU100TF lug for the FA, FH, and FC breakers?

#12-#3 AWG Str (2.5-35 mm2)
#12-#8 AWG Sol (2.5-10 mm2)


CTA-ID : 6430
Was this helpful?
What can we do to improve the information ?