Technical FAQs

Ask a Question

What wire-binding torque should be applied to the AL100FA4 lug for the FC and FCL breakers?

65 lb-in (7 N-m) for all wire sizes
#14-#3 AWG Str (2.5-35 mm2)
#14-#8 AWG Sol (2.5-10 mm2)
#8-#1 AWG Str (10-50 mm2)
#12-#10 AWG Sol (2.5-6 mm2)


CTA-ID : 6424
Was this helpful?
What can we do to improve the information ?