Technical FAQs

Ask a Question

Which wire sizes will the CU250KA lug for the circuit breakers KA, KH, KC, KI accept?

#4 AWG-250 kcmil (25-120 mm2) copper only





CTA-ID : 6406
Was this helpful?
What can we do to improve the information ?