Technical FAQs

Ask a Question

What are the repair parts for a T327N Series E01 General Duty Safety Switch?

Issue:
Repair parts

Product Line:
GD Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 40510-512-50
Load base assembly - 40510-511-50
Arc supressor - 40510-574-02
Neutral assembly - 40510-507-50
Base assembly mounting screws - 21427-202-41 (6) required for line base & (7) required for load base.
Arc supressor mounting screw - 40205-082-01
Neutral bonding strap assembly - 40283-312-50
Neutral assembly mounting screw - 40205-065-01 (4) required
Cross Arm Insulator - 40510-308-01 (insulator) and 40510-318-01 (dust shield - retainer for insulator)


CTA-ID : 8352
Was this helpful?
What can we do to improve the information ?