Technical FAQs

Ask a Question

What are the repair parts for a DU326 Series E01 & E03 General Duty Safety Switch?

Issue:
Repair parts

Product Line:
GD Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 40510-440-51
Arc supressor - 40510-574-02
Lug assembly - 8011612250
Base assembly mounting screws - 21427-202-41 (6) required for line base
Arc supressor mounting screw - 40205-082-01
Lug mounting nut - 23427-028-00
Cross Arm Insulator - 40510-308-01 (insulator) and 40510-318-01 (dust shield - retainer for insulator)



CTA-ID : 8351
Was this helpful?
What can we do to improve the information ?