Technical FAQs

Ask a Question

What are the repair parts for a D325N Series E03 General Duty Safety Switch?

Issue:
Repair parts

Product Line:
GD Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 40510-627-50
Load base assembly - 40510-628-50 (Includes Neutral Assembly)
Arc supressor - 40510-574-02
Lug assembly - 40251-136-50
Neutral assembly - 40510-630-50
Base assembly mounting screws - 21427-202-41 (6) required for line base & (7) required for load base.
Arc supressor mounting screw - 40205-082-01
Neutral mounting screw - 21404-202-00 (2) required
Neutral mounting washer - 23602-117-01 (2) required
Lug mounting nut - 23427-028-00
Neutral bonding assembly - 40283-185-82
Cross Arm Insulator - 40510-308-01 (insulator) and 40510-318-01 (dust shield - retainer for insulator)



CTA-ID : 8342
Was this helpful?
What can we do to improve the information ?