Technical FAQs

Ask a Question

What are the repair parts for a 82352, Series E1 Double throw Safety Switch?

The parts listed here are the only field replaceable parts.
Blade assembly - 40538-424-50
Top switch base assembly - 40538-425-50
Bottom switch base assembly - 40538-426-50
Handle knob assembly - 40284-357-50
Cover interlock assembly - 116101
Lug assembly - 40251-016-52
base mounting screws - 21427-171-61
Cover interlock Key - 190002
Cover interlock assembly mounting screws - (1) 21422-171-01 & (2) 21427-171-61


CTA-ID : 5732
Was this helpful?
What can we do to improve the information ?