Technical FAQs

Ask a Question

What are the wire binding screw torque requirements for the UL listed CK type breaker?

Torque requirement is 375 in/lb (1200A) or 275 in/lb (800A)



CTA-ID : 5697
Was this helpful?
What can we do to improve the information ?