Technical FAQs

Ask a Question

What is the wire binding torque requirements for the NC100H M9 accessories?<br />

For MX shunt trip, OF auxiliary switch, MN undervoltage release, and SD alarm contact, torque is 0.8 N-m or 7.1 lb.-in.



CTA-ID : 5691
Was this helpful?
What can we do to improve the information ?