Technical FAQs

Ask a Question

Replaced ATV16 and need to know where is the FW terminal on the Altivar ATV18 drive?

Issue: Replaced ATV16 and need to know where is the FW terminal on the Altivar ATV18 drive?
 
Product Line: ATV18
 
Environment: All
 
Cause: Control wiring
 
Resolution: The FW terminal on ATV16 is same as LI1 on ATV18.


 
Was this helpful?
What can we do to improve the information ?