Technical FAQs

Ask a Question

Where would you wire in an emergency stop on the Altivar ATV18.

Issue: Where would you wire in an emergency stop on the Altivar ATV18.
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: Can put it between LI1 forward and +24 since will only be running in forward direction.


 
Was this helpful?
What can we do to improve the information ?