Technical FAQs

Ask a Question

Will the Altivar ATV18 drive receive an analog input?

Issue: Will the Altivar ATV18 drive receive an analog input?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: Yes. It will receive 0-10 vdc and 0,4-20 mA. Standardly it is summed.


 
Was this helpful?
What can we do to improve the information ?