Technical FAQs

Ask a Question

How I do set a speed reference on the Altivar ATV18 without using a speed pot?

Set the low speed. This can be set up to the high speed setting. The drive will follow this reference when run command is given.


CTA-ID : 4338
Was this helpful?
What can we do to improve the information ?