Technical FAQs

Ask a Question

Is it normal for the Altivar ATV18 on power up shows RDY, then it go to ref freq. ( reference frequency ) when started?

Yes, even if you are displaying another parameter on power down, when it is powered up it comes up with RDY if LI1 is made and it then goes to a frequency ref. when started.

CTA-ID : 4327
Was this helpful?
What can we do to improve the information ?