Technical FAQs

Ask a Question

Can the Altivar ATV16 speed be adjusted from the keypad?

Issue: Can the Altivar ATV16 speed be adjusted from the keypad?
 
Product Line: ATV16
 
Environment: All
 
Cause: N/A
 
Resolution: Yes by using the up and down arrows if have the VW3A16102 option and it is set up for local control allowing access to LFr parameter. Otherwise can adjust the speed using LSP and HSP if using this as speed reference and have either no voltage on AIV or full 10v present there.


 
Was this helpful?
What can we do to improve the information ?