Technical FAQs

Ask a Question

What is the difference between a FHL and FHP breaker?

FHL breaker has lugs on line and load side, the FHP has lugs on the load side only. The FHP is also provided with `P` screws to secure the base to the cover.

CTA-ID : 2526
Was this helpful?
What can we do to improve the information ?