Technical FAQs

Ask a Question

What are the repair parts for a HNP320RGFI, Series 002 Hitch-N-Post Branch Plug-On Unit?

The Hitch-N-Post product line is obsolete and no longer being manufactured. There are no field replaceable parts available for the HNP320RGFI, except for the QO120GFI circuit breaker and the 125 volt/20 amp receptacle (4054001450). However, this complete Plug-On Unit may still be available. Please check availability for a complete HNP320RGFI through a local Square D Authorized distributor.


CTA-ID : 5665
Was this helpful?
What can we do to improve the information ?