Technical FAQs

Ask a Question

Why is the Altivar ATV16 unit is flashing 888 (possible may show some other undocumented dislay) because the keypad is located on the drive?

Issue: Why is the Altivar ATV16 unit is flashing 888 (possible may show some other undocumented dislay) because the keypad is located on the drive?
 
Product Line: ATV16
 
Environment: All
 
Cause: Display flashing 888
 
Resolution: The switch mode power supply has probably failed. Will need a new drive.


 
Was this helpful?
What can we do to improve the information ?