Technical FAQs

Ask a Question

What are the repair parts for an EZMH314125, Series M01 branch unit?

Issue:
Current design repair parts

Product Line:
EZM Metering

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:

Customer Cover (includes labels) - EZM314125C
Cover Screws - 4020513002K
Meter Socket Cover (cover for one meter position) - MMRC
Parts Kit (one position, meter socket line side through tenant breaker base) - MM125KIT
Horn Bypass Kit (includes parts for one meter socket position) - MMHB
Circuit Breaker RB Cover (one position) - BCV
Enclosure connecting hardware and Service Disconnect labels - 7329791750
Mounting Channel - 7329772301
Equipment Ground Bar Assembly
Ground Bar - 7329729850
Mounting Bracket - 7329653201
Ground Bar Mounting Screws - (2) 2142217101
Bracket Mounting Screws - (2) 2153217161
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP
Top Endwall Rain Cap – 7329714601
Top Endwall Rain Cap Mounting Screws – 4020513002K (Includes 10 screws; only 2 screws are used to secure the rain cap)


 
Was this helpful?
What can we do to improve the information ?