Technical FAQs

Ask a Question

What is the part number of the speed potentiometer that is used for the Omegapak 8804 unit?

It is a Class 9001, Type K2107 This is the speed pot.


CTA-ID : 4180
Was this helpful?
What can we do to improve the information ?