Technical FAQs

Ask a Question

Will the snubber assembly part number 52011-241-53 (book calls for a -55) for a larger 100hp drive work on the Omegapak 8804 60 hp, C frame, VT?<br />

Yes, you can use the snubber assembly from the larger drive on this smaller one.


CTA-ID : 4155
Was this helpful?
What can we do to improve the information ?