Technical FAQs

Ask a Question

Is there an assembly that can house filters to keep the dust out of the fan on the front of 300hp Omegapak 8804 unit?

There is not a kit for this. There is a modification that can be done in the factory at the time it is ordered so it can be done. Will have to get field services to go out to site to install it.


CTA-ID : 4117
Was this helpful?
What can we do to improve the information ?