Technical FAQs

Ask a Question

What are the compatible revisions between serial communication and DOI memory revision for the Omegapak 8804 with DOI (digital operator interface)?

The serial communication memory revision B is compatible with DOI module (memory chip) revision A-E, serial communication memory revision C is compatible with DOI module (memory chip) revision F-G, serial communication memory revision D is compatible with DOI module (memory chip) revision F-G, serial communication memory revision E & F is compatible with DOI module (memory chip) revision H


CTA-ID : 4103
Was this helpful?
What can we do to improve the information ?