Technical FAQs

Ask a Question

What is the Omegapak 8804 service bulletin part number of the Type MC-15 ( Type CT Controller - Mod T07 { part number 52011-417 }) stepped reference option board for use with Constant Torque ( Type CT ) omegapak?

8804-54 is the part number of the manual.


CTA-ID : 4095
Was this helpful?
What can we do to improve the information ?