Technical FAQs

Ask a Question

What are the repair parts for an EZM312200, Series M01 branch unit?

Issue:
Repair parts

Product Line:
EZM Metering

Environment:
Repair parts

Cause:
Maintenance
Only the parts listed below are considered field replaceable:

Customer Cover (includes labels) - EZM312200C
Cover Screws - 4020513002K
Meter Socket Cover (cover for one meter position) - MMC
Meter Socket Sealing Ring (aluminum latch type) - 2920910001
Blank Cover above top meter position - MMCBK
Spacer Cover above top blank cover position - EZM23TBKC
Parts Kit (one position, meter socket line side through tenant breaker base) - MM200KIT
Circuit Breaker RB Cover (one position) - BCV
Enclosure connecting hardware and Service Disconnect labels - 7329791750
Mounting Channel - 7329772401
Equipment Ground Bar Assembly
Ground Bar - 7329729850
Mounting Bracket - 7329653201
Ground Bar Mounting Screws - (2) 2142217101
Bracket Mounting Screws - (2) 2153217161
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP


CTA-ID : 3033
Was this helpful?
What can we do to improve the information ?