Technical FAQs

Ask a Question

What are the repair parts for a QO318L200GRB, Series S02, Load Center?

Issue:
Product design repair parts

Product Line:
QO Three Phase Load Centers

Environment;
Repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered replaceable.
Cover - 4056317550
Interior Trim with Labels - 4056313501K
Interior Assemebly - QO318L200RBI
Neutral Bonding Screw - 4028344850K
Main Lugs - QOL3225
Interior Trim Mounting Screw - 4020513001K
RB Door Mounting Screws - 2142217101
Outdoor Cover Latch - 4056314701
Outdoor Cover Latch Rivet - 2410212160
Main Lug Mounting Keps Nut  - 2342702000
Equipment Ground Bar - PK23GTA and LK100AN


CTA-ID : 5503
Was this helpful?
What can we do to improve the information ?