Technical FAQs

Ask a Question

Where on the Omegapak 8804 can you obtain an analog output representing current so can get a 4-20mA output?

There is a 0-5V signal on pins 30 and 31 for 0-150%. Told him he would have to get a convertor to change this to a 4 -20ma source.


CTA-ID : 4069
Was this helpful?
What can we do to improve the information ?