Technical FAQs

Ask a Question

Which terminals on the Omegapak 8804 bypass the OT fault?

Can jumper terminals 18 to 22 (internal temperature switches and precharge contactor) and 18 to 28 (external temperature switch if used) would bypass the OT. Need to be aware that it is faulting for a reason though if occurring and would not try to run with these jumpers installed and this is only for test purposes.


CTA-ID : 4059
Was this helpful?
What can we do to improve the information ?