Technical FAQs

Ask a Question

Where do you wire the speed potentiometer on the Omegapak 8803 Type P unit?

The Speed pot is wired on terminals OE1, E1, P10 . The wiper goes to E1 terminal, P10 is the +10v and OE1 is com (0v).

CTA-ID : 4045
Was this helpful?
What can we do to improve the information ?