Technical FAQs

Ask a Question

Do the cooling fans come on when you power up the Omegapak 8803 or are they temperature controlled?

The cooling fans on this unit should turn on when line power is applied to the drive and they are operating properly.



CTA-ID : 4036
Was this helpful?
What can we do to improve the information ?