Technical FAQs

Ask a Question

What are the repair parts for a QO13040M200, Series S1 (or S01), Load Center?

Issue:
Design repair parts

Product Line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - QOC30UF/S
Interior Assembly - QO13040M200I
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QOM2200VH
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K
Door Latch Kit 4020284450K
Main Circuit Breaker and Main Lugs Keps Nuts - 2342702001



CTA-ID : 2976
Was this helpful?
What can we do to improve the information ?