Technical FAQs

Ask a Question

What are the repair parts for a QO12024L125G, Series S01?

Issue:
Current design repair parts

Product Line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - QOC24UF/S or QOC20U100F/S - Design change in Feb. of 2016 moved this load center from box 7 (uses cover QOC24UF/S) to box 6 (uses cover QOC20U100F/S).  Select the appropriate cover based on the dimensions of the load center. Box dimensions below.
Interior Assembly - QO12024L125GI
Neutral Bonding screw - 4028345850K
Main Lugs - QOL125
Indoor Cover mounting screw - 4020513002K
Indoor Cover Hinge - 4028356450K (Kit contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Main circuit breaker and main lugs keps nut - 2342702001


Box dimensions:
Box 6: 14.25" x 17.92" x 3.75"
Box 7: 14.25" x 20.92" x 3.75"
Was this helpful?
What can we do to improve the information ?