Technical FAQs

Ask a Question

What are the repair parts for a PAK75PG, Series E01, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Panel Cover - 4054025101
Panel Cover Mounting Screw - (2) 2142717161
Pedestal Cover - 4054013801
Pedestal Cover Mounting Screw - (2) 4020513001K
Interior Trim - 4054024701
Interior Trim Mounting Screw - (2) 4020513001K
Interior Assembly - 4054020250 (Does NOT include Base Assembly, see below. Includes Circuit Breaker(s) and Receptacles(s) below).
Base Assembly - 4054008650
Circuit Breaker - QO120GFI, QO130 and QO2505212
Receptacle - 4054001450 (125 volt/20 amp), 4054004450 (125 volt/30 amp) and 4053901901 (Obsolete - replaced by 4054027950 (125/250 volt/50 amp)
Loop Feed Phase/Neutral Lugs Assembly - 4054014551
Loop Feed Lugs Assembly Mounting Screw - (4) 2159417121
Loop Feed Ground Lug - (2) 4025104251, Mounting Screw - (2) 4020600903
Neutral Bonding Screw - Not Applicable
NOTE: Covers and Interior Trims do not have labels applied.



CTA-ID : 5491
Was this helpful?
What can we do to improve the information ?