Technical FAQs

Ask a Question

What are the repair parts for an EZM11600CB, Series M01 main circuit breaker unit?

Only the parts listed below are considered field replaceable:

Cover (full length) - EZM11600CBC
Cover Screws - 4020513002K
Main Circuit Breaker - PAF2026
Rating Columns for Circuit Breaker - RC21600RC
Line Lugs (6 per Phase and Neutral) - AL2500PA
Bonding Strap - 7329696751
Mounting Channel - 7329654302
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP

CTA-ID : 3330
Was this helpful?
What can we do to improve the information ?