Technical FAQs

Ask a Question

What are the repair parts for a HOM48L125GRB, Series 1(or 001) load center?

Issue:
Current design repair parts

Product line:
Homeline load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4055333450 (includes the cover latch)
Cover Mounting Screw - 2142717161 (2 required)
Interior Trim - 4055844901
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4055845250
Main Lugs - Order Interior Assembly
Neutral Bonding Screw - 4020502001
Equipment Ground Bar - PK7GTA
Note: Replacement interior trims and covers DO NOT come with labels.


CTA-ID : 2942
Was this helpful?
What can we do to improve the information ?