Technical FAQs

Ask a Question

What are the repair parts for a QMB261H, Series D2 (D02)?

The QMB device is a single switch, meaning it contains one switch in the one device. Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly (1 required) - 4056669451
Load Base Assembly (1 required, includes lugs) - 4056002650
Handle Knob Kit - 4028343750
Lug Assembly (per lug) - 4025101652

CTA-ID : 2444
Was this helpful?
What can we do to improve the information ?