Technical FAQs

Ask a Question

What are the repair parts for a QMB221H, Series D2 (D02)?<br />

The QMB device is a single switch, meaning it contains one switche in the one device. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly (1 required) - 4051254201
Handle Knob Kit - 4028343750
Lug Assembly (per lug) - 4025101652




CTA-ID : 2422
Was this helpful?
What can we do to improve the information ?