Technical FAQs

Ask a Question

What are the repair parts for a PAK61P, Series E01, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Panel Cover - 4054025101
Panel Cover Mounting Screw - (2) 2142717161
Pedestal Cover - 4054013801
Pedestal Cover Mounting Screw - (2) 4020513001K
Interior Trim - 4054024001
Interior Trim Mounting Screw - (2) 4020513001K
Interior Assembly - Not Available. Order Base Assembly, Circuit Breaker(s) and Receptacle(s) shown below)
Base Assembly - 4054013950
Circuit Breaker - QO120 and (2) QO130
Receptacle - 4054001450 (125 volt/20 amp) and (2) 4054004450 (125 volt/30 amp)
Loop Feed Phase/Neutral Lugs Assembly - 4054014550
Loop Feed Lugs Assembly Mounting Screw - (4) 2159417121
Loop Feed Ground Lug - (2) 4025104251, Mounting Screw - (2) 4020600903
Neutral Bonding Screw - Not Applicable
NOTE: Covers and Interior Trims do not have labels applied.



CTA-ID : 5456
Was this helpful?
What can we do to improve the information ?