Technical FAQs

Ask a Question

What are the repair parts for a QO318L200G, Series S1, Load Center?

Only the parts listed below are considered field replaceable.
Cover - QOC30UF/S
Interior Assembly - QO318L200I
Neutral Bonding Screw - 4028344850K
Main Lugs - QOL3225
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K
Door Latch Kit - 4020284450K
Main Circuit Breaker and Main Lugs Keps Nut - 2342702000
Equipment Ground Bar - PK23GTA and LK100AN

CTA-ID : 3290
Was this helpful?
What can we do to improve the information ?