Technical FAQs

Ask a Question

What are the repair parts for a HOM48L125GC, Series 001 (or 1) load center?

Issue:
What are the repair parts for a HOM48L125GC, Series 001 (or 1) load center?

Product Line:  
Indoor Homeline Main Lug Load Centers

Environment:  
Maintenance

Cause:  
Product repairs 

Resolution

Only the parts listed below are considered field replaceable.
Cover - 4055844801 (Replacement covers DO NOT have labels, may consider purchasing a new load center)
Cover Mounting Screw - 4020513002K
Interior Assembly - 4055845250
Main Lugs - Order Interior Assembly
Neutral Bonding Screw - 4020502001
Equipment Ground Bar - PK7GTA



CTA-ID : 2938
Was this helpful?
What can we do to improve the information ?