Technical FAQs

Ask a Question

What are the repair parts for a QMB263T, Series D2 (D02)?

The QMB device is a twin switch, meaning it contains two switches in the one device. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Complete Arc Suppression Assembly - 3 part numbers required:
(1) Arc suppressor Assembly (1 required) - 4052021450
(1) Arc Shield (top cover) (1 required) - 4052017302
(2) Push nuts (2 required) - 2330241601
Load Base Assembly (1 required, includes lugs) - 4052021651
Load Base Mounting Screw (2 required per load base) - 4020506501
Handle Knob Kit - 4028343750
Lug Assembly (per lug) - 4025101851
Lug Mounting Nut (per lug) - 2342702001


CTA-ID : 2915
Was this helpful?
What can we do to improve the information ?