Technical FAQs

Ask a Question

What are the repair parts for a PAK11P, Series E01, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Panel Cover - 4054005101
Panel Cover Mounting Screw - (2) 2142717161
Pedestal Cover - 4054013801
Pedestal Cover Mounting Screw - (2) 4020513001K
Interior Trim - 4054008101
Interior Trim Mounting Screw - (2) 4020513001K
Interior Assembly - 4054018550 (Includes Base Assembly, Circuit Breaker(s) and Receptacle(s) shown below)
Base Assembly - 4054014050
Circuit Breaker - (2) QO120
Receptacle - (2) 4054001450 (125 volt/20 amp)
Loop Feed Phase/Neutral Lugs Assembly - 4054013550
Loop Feed Lugs Assembly Mounting Screw - (4) 2159417121
Loop Feed Ground Lug - (2) 4025104251, Mounting Screw - (2) 4020600903
Neutral Bonding Screw - Not Applicable
NOTE: Covers and Interior Trims do not have labels applied.



CTA-ID : 5440
Was this helpful?
What can we do to improve the information ?