Technical FAQs

Ask a Question

What are the repair parts for a QO1816M150FTRB, Series S2, Load Center?

Only the parts listed below are considered field replaceable.
Cover - 4056317550
Interior Trim with Labels - 4056313401K
Interior Assembly - QO1816M150FTRBI
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QOM2150VH
Interior Trim Mounting Screw - 4020513001K
RB Door Mounting Screws - 2142217101
Outdoor Cover Latch - 4056314701
Outdoor Cover Latch Rivet - 2410212160
Main Circuit Breaker and Main Lugs Keps Nut - 2342702001

CTA-ID : 3281
Was this helpful?
What can we do to improve the information ?