Technical FAQs

Ask a Question

Can the UL listed Multi 9 CB`s be used on a 240Vac delta system?

Yes. 5kA single pole AIR; 10kA AIR for 2 and 3 pole.


CTA-ID : 3276
Was this helpful?
What can we do to improve the information ?