Technical FAQs

Ask a Question

What are the repair parts for a QO12030M150RB, Series S2 (or S02), Load Center?

Issue:
Design repair parts

Product Line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4056317650
Interior Trim with Labels - 4056313102K
Interior Assembly - QO12030M150RBI
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QOM2150VH
Interior Trim Mounting Screw - 4020513001K
RB Door Mounting Screw - 2142217101
Main Circuit Breaker and Main Lug Keps Nut - 2342702001
Outdoor Cover Latch - 4056314701
Outdoor Latch Rivet - 2410212160


CTA-ID : 2909
Was this helpful?
What can we do to improve the information ?